BlogDepthAI-v2Releases

DepthAI 2.27.0 released

Hello community.

We have released a minor update to the DepthAI library. The changelog is available here:

Features

  • Automatic crash dump collection when DEPTHAI_ENABLE_FEEDBACK_CRASHDUMP is set.

Bug Fixes

  • Fix PointCloud generation when depth comes out of the ImageAlign node
  • Fix IMX214 (OAK Lite series) potential crash on init with more complex pipelines
  • Fix a rare bug on a crash if a camera stream is closed after 1 second while AF is running

Python Only

  • Add support for NumPy 2

Comments (0)

Hello community.

We have released a minor update to the DepthAI library. The changelog is available here:

Features

  • Automatic crash dump collection when DEPTHAI_ENABLE_FEEDBACK_CRASHDUMP is set.

Bug Fixes

  • Fix PointCloud generation when depth comes out of the ImageAlign node
  • Fix IMX214 (OAK Lite series) potential crash on init with more complex pipelines
  • Fix a rare bug on a crash if a camera stream is closed after 1 second while AF is running

Python Only

  • Add support for NumPy 2
MartinMotycka changed the title to DepthAI 2.27.0 released .
2 months later